The N7626C Signal Studio Pro for LTE V2X 2024 Update 1.0 software enables you to add waveforms from the software's WaveformLibrary to evaluate multi-standard radio (MSR) effects on LTE V2X signals.
Click this button to open a
drop-down menu
from which you can select a carrier to add to the setup table. The carrier
is inserted above the currently selected row in the table. The maximum
number of carriers is 16.
Click this button to delete the currently selected carriers in the setup table. You can highlight multiple carriers for deletion by holding down the CTRL key. You can also use the SHIFT key to select a succession (group) of carriers.
Click this button to quickly add a copy of the selected carrier to the last row in the setup table.
Double-click or use the drop-down menu to control the operating state of the carrier.
Selects the waveform file.
Shows the source sampling rate of the waveform. You cannot edit this cell.
Shows the source Waveform Length, in points. You cannot edit this cell.
Waveform Length is directly related to the Oversampling Ratio value selected. The higher the Oversampling Ratio, the larger the waveform.
Selects the baseband sample rate.
View the Waveform Length, displayed in points. You cannot edit this cell.
Waveform Length is directly related to the Oversampling Ratio value selected. The higher the Oversampling Ratio, the larger the waveform.
Set the frequency offset for the carrier relative to the signal generator’s frequency setting.
The range of the parameter is coupled to the Baseband Sampling Rate and the max ARB Sample Clock of the connected signal generator.
Range: -60 to 0 dB
Set the carrier’s power relative to the signal generator’s amplitude setting.
Range: 0 to 100000
Default: 0
Set the timing offset of the carrier with number of base sampling duration (1/30.72MHz).
Range: 0 to 359 degrees
Set the initial phase of the carrier.
Range: 1 to 20
Set the filter ratio. this will apply to source waveform filter.
The graph view displays several different representations of the generated waveform. For more information, see Graph View.